~!#🔥⚽"DIRECT/LIVE"!! Inter Barcelone en direct streaming! Ligue 1 2025 Direct 06 may 2025 54601

Inter Milan - FC Barcelone en direct : vers un match retour aussi fou que l'aller ? Après une demi-finale aller endiablée, qui de l'Inter Milan de Marcus Thuram ou du FC Barcelone de Lamine Yamal se qualifiera pour la finale de la Ligue des champions ? Suivez ce match décisif avec notre direct The players know they take risks by going out because today there is social media but all of them were perfect. One of the most intriguing showdowns between team-mates will see Jorginho go up against fellow Chelsea midfielder N'Golo Kante. It is why he made a detour to USA before even setting foot on Polish soil. That first meeting was close to four hours, Sousa tells Sky Sports. With two winners in the last month and over and given away in prizes, could you be the next player to land the quarter of a million pounds? Again, though, Maggiore felt compelled to make a big call; to do right by himself. Doing so certainly did not hinder his development; if anything, it helped. Some people will think I’m stupid for saying that, but we have that belief and confidence that we can win it. Not many people on the outside will think that but I’m sure everyone in this dressing room – the players, the staff and the management – all have that same belief that we can. Rashford, however, insists there are no truth to those rumours and that he is focused on improving his own game.

""~!#🔥⚽"DIRECT/LIVE"!! Inter Barcelone en direct streaming! Ligue 1 2025 Direct 06 may 2025

""~!#🔥⚽"DIRECT/LIVE"!! Inter Barcelone en direct streaming! Ligue 1 2025 Direct 06 may 2025

| 1h 29m 29s | Video has closed captioning.

Inter Milan - FC Barcelone en direct : vers un match retour aussi fou que l'aller ? Après une demi-finale aller endiablée, qui de l'Inter Milan de Marcus Thuram ou du FC Barcelone de Lamine Yamal se qualifiera pour la finale de la Ligue des champions ? Suivez ce match décisif avec notre direct

Aired: 30 March 2024